Description of multi_role_processParamUpdate is incorrect

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Low
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-1772
    • BLE Stack BLE5-2.1.1
    • Hide
      BLE Stack BLE5-2.1.3 RC1
      BLE Stack BLE5-2.1.3
      Show
      BLE Stack BLE5-2.1.3 RC1 BLE Stack BLE5-2.1.3

      Installer: simplelink_cc13x2_26x2_sdk_3_40_00_02

      File:

      • - C:\ti\simplelink_cc13x2_26x2_sdk_3_40_00_02\examples\rtos\CC26X2R1_LAUNCHXL\ble5stack\multi_role\Application\multi_role.c
      • And for all other supported boards.

      Problem description:
      The description of the multi_role_processParamUpdate is obviously wrong:

      /*********************************************************************
       * @fn      multi_role_processParamUpdate
       *
       * @brief   Remove a device from the connected device list
       *
       * @return  index of the connected device list entry where the new connection
       *          info is removed from.
       *          if connHandle is not found, MAX_NUM_BLE_CONNS will be returned.
       */
      

      It doesn't describe this function, it's probably copied from a different function.
      (There is also a spelling error in one comment in this function were update is used instead of update.)

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2372 - Description of multi_role_processPa...
                ERROR
                • Last Sync Date: