gapBondMgr_ProcessAttErrRsp uses attribute handle for connection handle

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-1486
    • BLE Stack BLE5-2.1.0
    • Hide
      BLE Stack BLE5-2.1.3 RC1
      BLE Stack BLE5-2.1.3
      Show
      BLE Stack BLE5-2.1.3 RC1 BLE Stack BLE5-2.1.3

      Installer: simplelink_cc13x2_26x2_sdk_3_30_00_03

      Problem description:
      The function gapBondMgr_ProcessAttErrRsp() repeatedly uses pRsp->handle (which points to the attribute handle that generated this error) when it should use the connection handle.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2319 - gapBondMgr_ProcessAttErrRsp uses at...
                ERROR
                • Last Sync Date: