-
Type:
Bug
-
Status: Fixed
-
Priority:
Medium
-
Resolution: Fixed
-
Product:Code Composer Studio IDE
-
Internal ID:CCSIDE-3841
-
Found In Release:CCS_10.0.0
-
Fix In Release:CCS_10.2.0
-
Affected Platform/Device:Generic
When project commands like "cleanProject" are used for GIT projects, the command appears to be executed successfully but does not return immediately and eventually times out. This only happens when the label decorations for GIT is enabled and the project name accounts for the label decoration. For example, for a dirty GIT project, there is a preceding ">" icon before the project name that needs to be accounted for:
js:> cleanProject("> projectName")
This will successfully clean the projectName project but the command will hang and eventually timeout.
If label decorations for GIT is simply disabled so that there is no preceding ">" icon to account for, then the below command works fine:
js:> cleanProject("projectName")
This will also successfully clean the projectName project but the command will return immediately as expected.