ARM assembler relocations for MOVT symbol+offset are resolved incorrectly for non-TI object file

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-7356
    • Hide
      ARM_18.12.0.LTS
      ARM_20.2.0.LTS
      Show
      ARM_18.12.0.LTS ARM_20.2.0.LTS
    • Hide
      ARM_20.2.2.LTS
      ARM_18.12.7.LTS
      Show
      ARM_20.2.2.LTS ARM_18.12.7.LTS
    • default
    • Hide
      There doesn't seem to be a direct way to control the relocation type produced by gcc (though -Os inhibits use of MOVT), and probably not by other compilers, either, suggesting that the only workarounds are either to compile all object files with the TI compiler, or use the non-TI linker.
      Show
      There doesn't seem to be a direct way to control the relocation type produced by gcc (though -Os inhibits use of MOVT), and probably not by other compilers, either, suggesting that the only workarounds are either to compile all object files with the TI compiler, or use the non-TI linker.
    • Hide
      If the TI linker is used to link object files produced by another compiler, it may incorrectly interpret some relocation entries. The problem is with certain specific relocation types: those for MOVT instructions, that are REL but not RELA. The TI compiler does not produce those relocation types -- it uses RELA exclusively -- but gcc is known to produce REL.
      Show
      If the TI linker is used to link object files produced by another compiler, it may incorrectly interpret some relocation entries. The problem is with certain specific relocation types: those for MOVT instructions, that are REL but not RELA. The TI compiler does not produce those relocation types -- it uses RELA exclusively -- but gcc is known to produce REL.

      If the TI linker is used to link certain object files produced by a non-TI compiler, it may incorrectly interpret some relocation entries, and encode incorrect addresses into the linked output file.

      The problem lies with REL-type relocations for MOVT instructions. The ELF file format specification describes two kinds of relocations, REL and RELA. RELA relocations have all their data in a separate section; REL relocations have some data in a separate section and some encoded within the instruction subject to the relocation.

      ARM MOVT instructions have special relocation types, because of the way that MOVT and MOVW are used to assemble large constants. REL-type MOVT relocations end up being processed slightly differently than other relocations, and the TI linker did not implement that difference correctly.

      For TI tools, the bug doesn't matter, because the TI compiler never makes REL-type MOVT relocations; it only makes RELA-type, which have no problems. However, other compilers (gcc is known to be one) do make the problematic relocations, and linking those object files using the TI linker can trigger the bug.

      When to worry about this bug:
      1. Is the object file compiled with a TI compiler? If yes, then don't worry.
      2. Does the output of "armofd --obj_display=none,relocs" for the file contain a relocation whose type includes the string "MOVT"? If no, then don't worry.
      3. Look at the output of "armofd -x" for the object file. Find the section whose sh_type field is SHT_REL. A few lines down from the section-header info is a "<relocations>" segment; do any of the listed relocations have an r_type field that contains the string "MOVT"? If no, then don't worry. If yes, then worry, because the situation that triggers the bug exists in that file.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2258 - ARM assembler relocations for MOVT ...
                SYNCHRONIZED
                • Last Sync Date: