Project Import Wizard should provide description of duplicate project name error

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Code Composer Studio
    • CCDSK-3857
    • Hide
      CCS_9.1.0
      CCS_9.0.1
      CCS_8.3.1
      CCS_9.2.0
      CCS_9.0.0
      CCS_8.0.0
      CCS_8.1.0
      CCS_10.0.0
      CCS_8.2.0
      CCS_9.3.0
      CCS_8.3.0
      Show
      CCS_9.1.0 CCS_9.0.1 CCS_8.3.1 CCS_9.2.0 CCS_9.0.0 CCS_8.0.0 CCS_8.1.0 CCS_10.0.0 CCS_8.2.0 CCS_9.3.0 CCS_8.3.0
    • Generic

      When you try to import a project that has the same name as a project that is already in the workspace you get an error icon beside the project name but no reason.  In addition it should state the error reason at the top of the dialog just like the Project Wizard does or in a dialog like Resource Explorer does.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-2255 - Project Import Wizard should provid...
                SYNCHRONIZED
                • Last Sync Date: