Add UART configuration to sysconfig allowing to choose different UART driver

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Implemented
    • Priority: Medium
    • TI Device Drivers
    • TIDRIVERS-4027
    • TIDRIVERS_4_40_00
    • TIDRIVERS_5_10_00
    • Hide
      CC13x2
      CC26x2
      Show
      CC13x2 CC26x2

      There are currently two UART drivers for CC13X2 and CC26X2 – UARTCC26XX and UARTCC26X2. We need to add a configuration parameter to SysConfig that allows the user to choose which driver to use. The documentation should explain the differences.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2195 - Add UART configuration to sysconfig...
                SYNCHRONIZED
                • Last Sync Date: