Add PBMQ_enqHead() capability

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Implemented
    • Priority: High
    • Network Development Kit
    • NDK-379
    • NDK_3_75_00

      A possible use case is, within a NIMU send function, when DMA resources to tag a PBM packet is not available. Currently, if a DMA descriptor is not available, we have no option but drop the packet. Instead, PBMQ_enqHead can be used to just add the packet back to the readyQ and send the packet when DMA descriptor is available.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2141 - Add PBMQ_enqHead() capability
                SYNCHRONIZED
                • Last Sync Date: