CCS: Extreme flickering when resizing panel that shows Getting Started, SysConfig or Resource Explorer

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Composer Studio
    • CCDSK-3752
    • Show
      https://jxbrowser.support.teamdev.com/support/tickets/8337
    • CCS_9.2.0
    • CCS_10.4.0
    • Generic
    • Hide
      On Windows PCs, there is extreme flickering when resizing a panel that shows Getting Started, SysConfig or Resource Explorer.

      Whenever the panel is resized by dragging a splitter bar (e.g. between the "Project Explorer" and "Resource Explorer"), the panel changes quickly to black and then back to the panel contents. This happens continuously while dragging the splitter bar.

      When resizing the entire CCS main window, the same type of flickering only occurs when reducing the panel size, and then only in the area is about to be "removed".
      Show
      On Windows PCs, there is extreme flickering when resizing a panel that shows Getting Started, SysConfig or Resource Explorer. Whenever the panel is resized by dragging a splitter bar (e.g. between the "Project Explorer" and "Resource Explorer"), the panel changes quickly to black and then back to the panel contents. This happens continuously while dragging the splitter bar. When resizing the entire CCS main window, the same type of flickering only occurs when reducing the panel size, and then only in the area is about to be "removed".

      CCS: Extreme flickering when resizing panel that shows Getting Started, SysConfig or Resource Explorer

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-2079 - CCS: Extreme flickering when resizi...
                SYNCHRONIZED
                • Last Sync Date: