Under eabi, the cinit entry for zero fill an of uninitialized section has a length that is 1/2 of what it should be

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-6456
    • Hide
      C2000_20.2.0.beta
      C2000_18.1.0.LTS
      C2000_18.12.0.LTS
      Show
      C2000_20.2.0.beta C2000_18.1.0.LTS C2000_18.12.0.LTS
    • Hide
      C2000_20.2.0.beta
      C2000_18.12.4.LTS
      C2000_18.1.7.LTS
      Show
      C2000_20.2.0.beta C2000_18.12.4.LTS C2000_18.1.7.LTS
    • default
    • Initialise the problem variables to zero explicitly.
    • Hide
      Uninitialised variables in EABI mode are supposed to be implicitly initialised to zero. It is possible that C2000 programs will not fully initialise them; because of an error in converting from 16-bit bytes to 8-bit bytes, the size of the zero-initialised range (or ranges) may be only half the total size.
      Show
      Uninitialised variables in EABI mode are supposed to be implicitly initialised to zero. It is possible that C2000 programs will not fully initialise them; because of an error in converting from 16-bit bytes to 8-bit bytes, the size of the zero-initialised range (or ranges) may be only half the total size.

      Under eabi, the cinit entry for zero fill an of uninitialized section has a length that is 1/2 of what it should be

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1912 - Under eabi, the cinit entry for zer...
                SYNCHRONIZED
                • Last Sync Date: