[NVSCC26XX] Update "maximum flash writes before erase" documentation

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • TI Device Drivers
    • TIDRIVERS-3545
    • 3.80.01
    • CORESDK_4_10_00
    • Hide
      I was reviewing the NVSCC26XX doxygen (file:///C:/ti/simplelink_cc13x2_26x2_sdk_2_40_00_79/docs/tidrivers/doxygen/html/_n_v_s_c_c26_x_x_8h.html) and noticed that there is a typo in the “Note” below regarding max number of writes per flash row. The “page” should be “row” as the limitation applies to the flash row.

      I would also like to add a statement to the effect of “It is the system developer’s responsibility to comply with this limitation when performing write operations to the flash memory.”
      Show
      I was reviewing the NVSCC26XX doxygen ( file:///C:/ti/simplelink_cc13x2_26x2_sdk_2_40_00_79/docs/tidrivers/doxygen/html/_n_v_s_c_c26_x_x_8h.html ) and noticed that there is a typo in the “Note” below regarding max number of writes per flash row. The “page” should be “row” as the limitation applies to the flash row. I would also like to add a statement to the effect of “It is the system developer’s responsibility to comply with this limitation when performing write operations to the flash memory.”

      [NVSCC26XX] Update "maximum flash writes before erase" documentation

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1765 - [NVSCC26XX] Update "maximum flash w...
                SYNCHRONIZED
                • Last Sync Date: