Use of --debug_software_pipeline, in combination with duplicate source file names in different directories, causes parallel

XMLWordPrintable

    • Type: Bug
    • Resolution: Won't Fix
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-5953
    • Hide
      C6000_8.2.4
       C6000_8.3.1
      Show
      C6000_8.2.4  C6000_8.3.1
    • For source files with duplicate names, use file-specific options to set unique --asm_directory.
    • Hide
      This is a known limitation of the compiler. All assembly files will be saved in the same directory so there will be name collisions if source files have the same name. In the absence of parallel make, only the last compiled file with the duplicate name will be saved.
      Show
      This is a known limitation of the compiler. All assembly files will be saved in the same directory so there will be name collisions if source files have the same name. In the absence of parallel make, only the last compiled file with the duplicate name will be saved.
    • This is standard compiler behavior. Please see recommended workaround.

      Use of --debug_software_pipeline, in combination with duplicate source file names in different directories, causes parallel

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1760 - Use of --debug_software_pipeline, i...
                SYNCHRONIZED
                • Last Sync Date: