Using --openmp:device and an improperly-declared target variable causes C6000 compiler to fail with INTERNAL ERROR: acpia6x experienced a segmentation fault

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-5903
    • Hide
      C6000_8.2.0
      C6000_8.3.0
      Show
      C6000_8.2.0 C6000_8.3.0
    • Hide
      C6000_8.3.5
      C6000_8.2.8
      Show
      C6000_8.3.5 C6000_8.2.8
    • None. It's still incorrect code, but with a horrendous error indication.
    • When using --openmp:device, if a target variable is not properly defined between omp "declare target" and "end declare target" pragmas, the compiler will crash. The code is incorrect, and the compiler should warn about it instead.

      Using --openmp:device and an improperly-declared target variable causes C6000 compiler to fail with INTERNAL ERROR: acpia6x experienced a segmentation fault

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1720 - Using --openmp:device and an impro...
                ERROR
                • Last Sync Date: