Compiler may crash when using attribute cc_rom

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-5578
    • MSP430_18.1.0.LTS
    • MSP430_18.1.5.LTS
    • Make sure the return value is used. Test the return value, or assign it to a dummy volatile variable.
    • When calling a cc_rom function that returns an int8_t value, the compiler may crash if the return value is ignored.

      Compiler may crash when using attribute cc_rom

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1686 - Compiler may crash when using attri...
                SYNCHRONIZED
                • Last Sync Date: