Local structure initialization is incorrectly optimized away

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-5527
    • Hide
      C6000_8.2.0
       ARM_18.1.0.LTS
       C2000_18.1.0.LTS
      Show
      C6000_8.2.0  ARM_18.1.0.LTS  C2000_18.1.0.LTS
    • Hide
      PRU_2.3.2
       ARM_18.1.6.LTS
       C2000_18.1.6.LTS
      Show
      PRU_2.3.2  ARM_18.1.6.LTS  C2000_18.1.6.LTS
    • None better than the one given in the description.
    • A program that saves the address of a variable in an initialised local struct, but does not use the variable directly, may lose ...

      Local structure initialization is incorrectly optimized away

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1629 - Local structure initialization is i...
                ERROR
                • Last Sync Date: