Global constexpr class errors out when assigning to member data

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-5486
    • Hide
      ARM_18.1.0.LTS
      MSP430_18.1.0.LTS
      C6000_8.3.0
      ARM_18.12.0.LTS
      ARM_19.6.0.STS
      MSP430_18.12.0.LTS
      MSP430_19.6.0.STS
      Show
      ARM_18.1.0.LTS MSP430_18.1.0.LTS C6000_8.3.0 ARM_18.12.0.LTS ARM_19.6.0.STS MSP430_18.12.0.LTS MSP430_19.6.0.STS
    • Hide
      MSP430_18.12.2.LTS
      ARM_18.1.6.LTS
      MSP430_18.1.6.LTS
      ARM_19.6.0.STS
      ARM_18.12.2.LTS
      C6000_8.3.4
      MSP430_19.6.0.STS
      Show
      MSP430_18.12.2.LTS ARM_18.1.6.LTS MSP430_18.1.6.LTS ARM_19.6.0.STS ARM_18.12.2.LTS C6000_8.3.4 MSP430_19.6.0.STS
    • Hide
      The error can be avoided If the constexpr class definition is wrapped in a function which simply returns the instance of the class.

      For example:
      constexpr MyClass getA()
      { MyClass A("This is a constant literal"); return A;}

      Using 'getA()' instead of 'A' will work as expected.
      Show
      The error can be avoided If the constexpr class definition is wrapped in a function which simply returns the instance of the class. For example: constexpr MyClass getA() { MyClass A("This is a constant literal"); return A;} Using 'getA()' instead of 'A' will work as expected.
    • Constexpr class definitions may generate spurious parser errors, including one about "accessing expired storage."

      Global constexpr class errors out when assigning to member data

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1614 - Global constexpr class errors out w...
                ERROR
                • Last Sync Date: