MISRA 12.2 is incorrectly issued when one variable is used multiple times as an array index in the same expression

XMLWordPrintable

    • Type: Bug
    • Resolution: Won't Fix
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-4943
    • Hide
      ARM_18.1.1.LTS
      ARM_18.12.0.LTS
      C2000_20.8.0.STS
      ARM_20.2.0.LTS
      C2000_20.2.0.LTS
      Show
      ARM_18.1.1.LTS ARM_18.12.0.LTS C2000_20.8.0.STS ARM_20.2.0.LTS C2000_20.2.0.LTS
    • No plans to address at this time.
    • MISRA 2004 checking has been deprecated. No further MISRA issues will be addressed.

      MISRA 12.2 is incorrectly issued when one variable is used multiple times as an array index in the same expression

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1485 - MISRA 12.2 is incorrectly issued wh...
                SYNCHRONIZED
                • Last Sync Date: