Install confirmation box should be clearer as to what preferences it refers to

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Implemented
    • Priority: Medium
    • Resource Explorer
    • REX-2039
    • Hide
      CCS_10.0.0
      CCS_9.3.0
      CCS_11.0.0
      CCS_11.1.0
      CCS_11.2.0
      REX_4.1.0
      CCS_12.5.0
      CCS_12.6.0
      CCS_12.3.0
      CCS_12.4.0
      CCS_12.1.0
      CCS_12.2.0
      CCS_12.0.0
      CCS_10.3.0
      CCS_10.4.0
      CCS_10.1.0
      CCS_10.2.0
      CCS_10.1.1
      CCS_12.7.0
      Show
      CCS_10.0.0 CCS_9.3.0 CCS_11.0.0 CCS_11.1.0 CCS_11.2.0 REX_4.1.0 CCS_12.5.0 CCS_12.6.0 CCS_12.3.0 CCS_12.4.0 CCS_12.1.0 CCS_12.2.0 CCS_12.0.0 CCS_10.3.0 CCS_10.4.0 CCS_10.1.0 CCS_10.2.0 CCS_10.1.1 CCS_12.7.0
    • Generic
    • N/A.
    • Hide
      When installing a SDK package using TI Resource Explorer, the Note in the message box says:
      Note: Install folder can be changed in preferences
      However, when using TI Resource Explorer from inside CCS, the text is confusing as it can lead for people to search in the global CCS Preferences instead of the Resource Explorer three-bar preference.
      The message could say instead:
      Note: Install folder can be changed in the Resource Explorer three-bar menu
      Show
      When installing a SDK package using TI Resource Explorer, the Note in the message box says: Note: Install folder can be changed in preferences However, when using TI Resource Explorer from inside CCS, the text is confusing as it can lead for people to search in the global CCS Preferences instead of the Resource Explorer three-bar preference. The message could say instead: Note: Install folder can be changed in the Resource Explorer three-bar menu

      Install confirmation box should be clearer as to what preferences it refers to

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1413 - Install confirmation box should be ...
                SYNCHRONIZED
                • Last Sync Date: