Macro with temp label causes assembler to crash

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-4668
    • Hide
      C6000_8.2.0
       C6000_8.1.0B1
       C2000_16.9.0.LTS
      Show
      C6000_8.2.0  C6000_8.1.0B1  C2000_16.9.0.LTS
    • Hide
      C6000_8.3.0
       ARM_18.9.0.STS
       C2000_18.9.0.STS
      Show
      C6000_8.3.0  ARM_18.9.0.STS  C2000_18.9.0.STS
    • The problem will not occur without macro labels. If labels are required, no workaround is known.
    • Hide
      The assembler may crash or report a memory misuse when using an assembly macro containing a label, if the label appears in an instruction in a position that requires extra lookahead to parse.

      The original example is a register name followed by a comma and a label use; for that assembler, the thing following the comma might be a shift specifier, so it requires expanding the macro label. That extra step frees some memory that it shouldn't, causing the problem.
      Show
      The assembler may crash or report a memory misuse when using an assembly macro containing a label, if the label appears in an instruction in a position that requires extra lookahead to parse. The original example is a register name followed by a comma and a label use; for that assembler, the thing following the comma might be a shift specifier, so it requires expanding the macro label. That extra step frees some memory that it shouldn't, causing the problem.

      Macro with temp label causes assembler to crash

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1385 - Macro with temp label causes assemb...
                ERROR
                • Last Sync Date: