Using the C interlister with C++14 features may generate error

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Code Generation Tools
    • CODEGEN-4581
    • Hide
      ARM_18.1.0.LTS
       MSP430_18.1.0.LTS
      Show
      ARM_18.1.0.LTS  MSP430_18.1.0.LTS
    • Hide
      ARM_18.1.2.LTS
       MSP430_18.1.2.LTS
      Show
      ARM_18.1.2.LTS  MSP430_18.1.2.LTS
    • Do not use the -s source interlisting option
    • Hide
      When using the -s C source interlisting option, the compiler may emit a bogus assembly directive for functions which do not have a body in the source code (e.g. certain implicit constructors). The assembler will emit an error when encountering this directive.
      Show
      When using the -s C source interlisting option, the compiler may emit a bogus assembly directive for functions which do not have a body in the source code (e.g. certain implicit constructors). The assembler will emit an error when encountering this directive.

      Using the C interlister with C++14 features may generate error

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1368 - Using the C interlister with C++14 ...
                SYNCHRONIZED
                • Last Sync Date: