ECC section names are randomly assigned

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-4251
    • ARM_16.9.3.LTS
    • ARM_18.1.0.LTS
    • Hide
      This happens in 16.9.X.LTS because the ECC initialization code iterates over an unsorted list. This list's order happens to be non-deterministic. The ECC code was refactored significantly before the 17.3 branch, and now uses a set, which is always ordered. Thus, the problem will not occur in 17.3.0.STS or any release thereafter. We do not plan to address this for the 16.9.X.LTS branch.
      Show
      This happens in 16.9.X.LTS because the ECC initialization code iterates over an unsorted list. This list's order happens to be non-deterministic. The ECC code was refactored significantly before the 17.3 branch, and now uses a set, which is always ordered. Thus, the problem will not occur in 17.3.0.STS or any release thereafter. We do not plan to address this for the 16.9.X.LTS branch.

      ECC section names are randomly assigned

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1036 - ECC section names are randomly assi...
                SYNCHRONIZED
                • Last Sync Date: