PRU compiler fails to account for zero-sized struct passed in register as function argument

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-4180
    • PRU_2.2.0
    • PRU_2.3.0
    • Hide
      If an empty struct is passed as a function argument, the caller function passes 0 in a register but the called function ignores the argument. This results in the subsequent argument being allocated to a different register than the one the caller used. Now, both caller and callee functions ignore zero-sized struct arguments.
      Show
      If an empty struct is passed as a function argument, the caller function passes 0 in a register but the called function ignores the argument. This results in the subsequent argument being allocated to a different register than the one the caller used. Now, both caller and callee functions ignore zero-sized struct arguments.

      PRU compiler fails to account for zero-sized struct passed in register as function argument

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1034 - PRU compiler fails to account for z...
                SYNCHRONIZED
                • Last Sync Date: