Assembler computes wrong result for expression 0x232800 % 0x10000

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-4113
    • Hide
      PRU_2.2.0
       C6000_8.2.0
       C2000_16.9.0.LTS
      Show
      PRU_2.2.0  C6000_8.2.0  C2000_16.9.0.LTS
    • Hide
      C6000_8.3.0
       C6000_8.2.3
       ARM_16.9.7.LTS
      Show
      C6000_8.3.0  C6000_8.2.3  ARM_16.9.7.LTS
    • In some instances, as in the original test case, the AND operator can be used instead, but that is not a general workaround.
    • The modulo operator in the TI assembler, for releases made in mid-to-late 2016 and all of 2017, is unreliable. In some cases it will produce an incorrect answer.

      Assembler computes wrong result for expression 0x232800 % 0x10000

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1028 - Assembler computes wrong result for...
                ERROR
                • Last Sync Date: