Linker takes over 5 minutes to finish

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-4078
    • Hide
      PRU_2.2.0
       C6000_8.2.0
       C2000_15.12.3.LTS
      Show
      PRU_2.2.0  C6000_8.2.0  C2000_15.12.3.LTS
    • Hide
      C6000_8.3.0
       C6000_8.2.3
       ARM_16.9.7.LTS
      Show
      C6000_8.3.0  C6000_8.2.3  ARM_16.9.7.LTS
    • None. If the linker command file wants to be that specific about memory ranges, then the work has to be done, and the option to disable the work has its own bug.
    • Hide
      Linking may take excessively long when the linker command file specifically places a lot of variables at specific addresses, especially for C2000. The original report was placing more than 300 variables. The --no_placement_optimization option is not a workaround because it causes a linker crash. Both problems are fixed together.
      Show
      Linking may take excessively long when the linker command file specifically places a lot of variables at specific addresses, especially for C2000. The original report was placing more than 300 variables. The --no_placement_optimization option is not a workaround because it causes a linker crash. Both problems are fixed together.

      Linker takes over 5 minutes to finish

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-1024 - Linker takes over 5 minutes to finish
                ERROR
                • Last Sync Date: