Writing multiple input sections in one line unexpectedly changes how input sections are combined into output sections

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-3918
    • Hide
      PRU_2.2.0
       C6000_8.2.0
       ARP32_1.1.0*
      Show
      PRU_2.2.0  C6000_8.2.0  ARP32_1.1.0*
    • Hide
      ARP32_1.1.0*
       ARP32_1.0.9
       C2000_18.1.0.LTS
      Show
      ARP32_1.1.0*  ARP32_1.0.9  C2000_18.1.0.LTS
    • Stick with separate lines, if there are subsection cases like this one that should be comprehended.
    • In a linker command file, using a line like "hello.obj (.const, .far)" may link differently than two lines with one section eac...

      Writing multiple input sections in one line unexpectedly changes how input sections are combined into output sections

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-984 - Writing multiple input sections in ...
                ERROR
                • Last Sync Date: