RPTB block containing RPT is too small

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-2176
    • Hide
      C2000_15.12.0.LTS
       C2000_16.9.0.LTS
      Show
      C2000_15.12.0.LTS  C2000_16.9.0.LTS
    • Hide
      C2000_17.6.0.STS
       C2000_16.9.3.LTS
      Show
      C2000_17.6.0.STS  C2000_16.9.3.LTS
    • Hide
      This bug can occur when there is a small loop containing a smaller loop, where the smaller loop behaves like memset(foo, 0, n). Only the fill value zero will trigger this bug. The generated RPTB may be one byte too small to be legal, and the assembler will reject the RPTB.
      Show
      This bug can occur when there is a small loop containing a smaller loop, where the smaller loop behaves like memset(foo, 0, n). Only the fill value zero will trigger this bug. The generated RPTB may be one byte too small to be legal, and the assembler will reject the RPTB.

      RPTB block containing RPT is too small

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-772 - RPTB block containing RPT is too small
                SYNCHRONIZED
                • Last Sync Date: