Warning "INLINE recursion limit exceeded" during RTS build

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-1649
    • Hide
      C6000_7.4.0B1
       C6000_8.1.0B1
       MSP430_15.12.0.LTS
      Show
      C6000_7.4.0B1  C6000_8.1.0B1  MSP430_15.12.0.LTS
    • Hide
      MSP430_4.4.8
       C6000_8.1.2
       MSP430_15.12.4.LTS
      Show
      MSP430_4.4.8  C6000_8.1.2  MSP430_15.12.4.LTS
    • None, for the automatic library builds. Elsewhere, one can use the hidden --inline_recursion_limit option to increase the limit above the default 10.
    • The compiler may emit the warning "INLINE recursion limit exceeded," but there is no way to suppress the warning, and it really isn't useful for the typical compiler user. These changes remove the warning.

      Warning "INLINE recursion limit exceeded" during RTS build

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-676 - Warning "INLINE recursion limit exc...
                SYNCHRONIZED
                • Last Sync Date: