INTERNAL ERROR for user code with void pointer dereference

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-49
    • SDSCM00008465
    • Hide
      C6000_7.4.0B1
      ARP32_1.0.0B1
      Show
      C6000_7.4.0B1 ARP32_1.0.0B1
    • Hide
      C6000_8.2.2
      C6000_8.1.5
      ARP32_1.0.9
      Show
      C6000_8.2.2 C6000_8.1.5 ARP32_1.0.9
    • Don't dereference pointers to type void
    • In relaxed mode, it is possible to write an expression that dereferences a void *. This doesn't mean anything, but if the user's code dereferences a volatile void *, the compiler could crash with an internal error.

      INTERNAL ERROR for user code with void pointer dereference

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-510 - INTERNAL ERROR for user code with v...
                SYNCHRONIZED
                • Last Sync Date: