Cortex-M0 library lacks uread4, etc.

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-573
    • SDSCM00046074
    • Hide
      ARM_15.12.0.LTS
      ARM_18.1.0.LTS
      ARM_16.9.0.LTS
      ARM_18.12.0.LTS
      ARM_5.2.0B1
      ARM_20.2.0.LTS
      Show
      ARM_15.12.0.LTS ARM_18.1.0.LTS ARM_16.9.0.LTS ARM_18.12.0.LTS ARM_5.2.0B1 ARM_20.2.0.LTS
    • Hide
      If using the TI compiler, the TI compiler doesn't call any of these functions, so no workaround should be necessary.
      If using any other vendor's compiler and linking with the TI toolchain, link with the other vendor's toolchain.
      Show
      If using the TI compiler, the TI compiler doesn't call any of these functions, so no workaround should be necessary. If using any other vendor's compiler and linking with the TI toolchain, link with the other vendor's toolchain.

      Cortex-M0 library lacks uread4, etc.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-467 - Cortex-M0 library lacks uread4, etc.
                SYNCHRONIZED
                • Last Sync Date: