Linker fails with internal error: lnk6x failed to allocate memory

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Code Generation Tools
    • CODEGEN-368
    • SDSCM00042581
    • Hide
      C6000_7.4.0B1
      ARP32_1.0.0B1
      Show
      C6000_7.4.0B1 ARP32_1.0.0B1
    • Hide
      ARP32_1.0.1
      C6000_7.4.3
      Show
      ARP32_1.0.1 C6000_7.4.3
    • Hide
      This bug can only be triggered if a partial link is performed using the
      --make_static, --localize or --hide option (the memory allocation
      failure will occur during the final link, however). Removing that option
      is one way to avoid this bug. Alternatively, the partial link step may
      be removed from the build process, if possible.
      Show
      This bug can only be triggered if a partial link is performed using the --make_static, --localize or --hide option (the memory allocation failure will occur during the final link, however). Removing that option is one way to avoid this bug. Alternatively, the partial link step may be removed from the build process, if possible.

      Linker fails with internal error: lnk6x failed to allocate memory

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-365 - Linker fails with internal error: l...
                SYNCHRONIZED
                • Last Sync Date: