Compilers on PC will not work without TMP set

XMLWordPrintable

    • Type: Bug
    • Resolution: Won't Fix
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-30
    • SDSCM00008248
    • Hide
      ARM_15.12.0.LTS
      C2000_16.9.0.LTS
      ARM_16.9.0.LTS
      C2000_6.4.0B1
      C2000_15.12.0.LTS
      MSP430_4.4.0B1
      C6000_8.1.0B1
      C6000_7.4.0B1
      MSP430_15.12.0.LTS
      ARM_5.2.0B1
      MSP430_16.9.0.LTS
      Show
      ARM_15.12.0.LTS C2000_16.9.0.LTS ARM_16.9.0.LTS C2000_6.4.0B1 C2000_15.12.0.LTS MSP430_4.4.0B1 C6000_8.1.0B1 C6000_7.4.0B1 MSP430_15.12.0.LTS ARM_5.2.0B1 MSP430_16.9.0.LTS
    • Hide
      Set the TMP environment variable, even if just set to . (current directory)


      Show
      Set the TMP environment variable, even if just set to . (current directory)
    • No longer relevant due to updated behavior

      When compiling on Windows operating systems, the code generator cannot find the icode file produced by the parser if the environment variable TMP is not
      set. If TMP is set, then all appears well.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-342 - Compilers on PC will not work witho...
                SYNCHRONIZED
                • Last Sync Date: