Disable diagnostic 1558 (--float_operations_allowed diagnostic) in standard header files

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-1026
    • SDSCM00051367
    • Hide
      ARM_15.12.0.LTS
      ARM_18.1.0.LTS
      ARM_16.9.0.LTS
      ARM_18.12.0.LTS
      ARM_20.2.0.LTS
      Show
      ARM_15.12.0.LTS ARM_18.1.0.LTS ARM_16.9.0.LTS ARM_18.12.0.LTS ARM_20.2.0.LTS

      The --float_operations_allowed option is used to identify floating point operations and issue an error if the user doesn't want them in the program. A program that includes math.h will generate diagnostics if either none or 32 is used as an argument. The emitting of the diagnostics is probably OK for none since users really shouldn't include math.h if no floating point is to be done, but it is a problem for 32-bit operations. If a user wants to only use 32-bit floating point, it is reasonable for them to include math.h. We should suppress the diagnostics from the standard header files.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-339 - Disable diagnostic 1558 (--float_op...
                SYNCHRONIZED
                • Last Sync Date: