The C2000 compiler produces the following instruction: MOV *+FP[AR0],SP

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-1084
    • SDSCM00051562
    • C2000_6.4.0
    • C2000_6.4.3
    • Hide
      There is no obvious workaround, but most like reducing the optimization
      level or adjusting the size/speed trade off (--opt_for_speed) will perturb the code enough to avoid the issue.
      Show
      There is no obvious workaround, but most like reducing the optimization level or adjusting the size/speed trade off (--opt_for_speed) will perturb the code enough to avoid the issue.

      The C2000 compiler produces the following instruction: MOV *+FP[AR0],SP

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-304 - The C2000 compiler produces the fol...
                SYNCHRONIZED
                • Last Sync Date: