Section relative ELF symbol values in partially linking object files should hold the section offset for the symbol

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-235
    • SDSCM00036874
    • Hide
      ARM_15.12.0.LTS
      ARM_18.1.0.LTS
      ARM_16.9.0.LTS
      ARM_18.12.0.LTS
      ARM_5.2.0B1
      ARM_20.2.0.LTS
      Show
      ARM_15.12.0.LTS ARM_18.1.0.LTS ARM_16.9.0.LTS ARM_18.12.0.LTS ARM_5.2.0B1 ARM_20.2.0.LTS

      The symbol value in an ELF relocatable file should be the offset from the beginning of the section. Typically the sections all start at address 0, so the value corresponds to its address in the file. In a partially linking object file, the sections will start at different addresses. The symbol values contain the absolute address instead of the offset.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-282 - Section relative ELF symbol values ...
                SYNCHRONIZED
                • Last Sync Date: