C2000 assembler segmentation fault on RPTB with syntax error

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-250
    • SDSCM00037411
    • C2000_6.4.0B1
    • C2000_15.12.0.LTS
    • Hide
      Ensure that RPTB statements follow the correct syntax:

      RPTB label, #immediate
      RPTB label, loc16

      If the #immediate or loc16 field is not present, the INTERNAL ERROR segmentation fault will occur. The line number given in the error message will be for a label.
      Show
      Ensure that RPTB statements follow the correct syntax: RPTB label, #immediate RPTB label, loc16 If the #immediate or loc16 field is not present, the INTERNAL ERROR segmentation fault will occur. The line number given in the error message will be for a label.

      C2000 assembler segmentation fault on RPTB with syntax error

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-267 - C2000 assembler segmentation fault ...
                SYNCHRONIZED
                • Last Sync Date: