EXIDX_CANTUNWIND yields invalid memory read

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-509
    • SDSCM00044735
    • C6000_7.4.0B1
    • C6000_7.4.1
    • Hide
      This bug can only occur when the program is terminating due to a
      problem with an uncaught exception. To work around the issue, ensure
      that C++ functions which might be called from a C function catch all
      exceptions.
      Show
      This bug can only occur when the program is terminating due to a problem with an uncaught exception. To work around the issue, ensure that C++ functions which might be called from a C function catch all exceptions.

      EXIDX_CANTUNWIND yields invalid memory read

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-246 - EXIDX_CANTUNWIND yields invalid mem...
                SYNCHRONIZED
                • Last Sync Date: