TMS570LC4357 ECC algorithm not supported

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Code Generation Tools
    • CODEGEN-1411
    • SDSCM00052814
    • Hide
      ARM_16.6.0.STS
       ARM_15.12.0.LTS
       ARM_5.2.0B1
      Show
      ARM_16.6.0.STS  ARM_15.12.0.LTS  ARM_5.2.0B1
    • Hide
      ARM_15.12.4.LTS
       ARM_5.2.9
       ARM_16.9.1.LTS
      Show
      ARM_15.12.4.LTS  ARM_5.2.9  ARM_16.9.1.LTS
    • Hide
      There is a backdoor in the implementation that you can use to realize this new algorithm. Use this algorithm specification:

      ECC {
      algo_name : address_mask = 0xffffffff
                  hamming_mask = /* address */
                                 0x53aaa750, 0xeb45d688,
                                 0xa6d54da8, 0x9e353c68,
                                 0x7e0cfc18, 0xfe03fc00,
                                 0x01fffc00, 0xfe0003f8,
                                 /* upper */
                                 0x2E4B2E4B, 0x57155715,
                                 0x99A699A6, 0xE338E338,
                                 0xFCC0FCC0, 0x00FF00FF,
                                 0xFF0000FF, 0xFF0000FF,
                                 /* lower */
                                 0xD1B4D1B4, 0x57155715,
                                 0x99A699A6, 0xE338E338,
                                 0xFCC0FCC0, 0x00FF00FF,
                                 0xFF0000FF, 0x00FFFF00,
                  parity_mask = 0x0c
                  mirroring = F021
      }

      If you value your sanity, do not ask where the constants come from.
      Show
      There is a backdoor in the implementation that you can use to realize this new algorithm. Use this algorithm specification: ECC { algo_name : address_mask = 0xffffffff             hamming_mask = /* address */                            0x53aaa750, 0xeb45d688,                            0xa6d54da8, 0x9e353c68,                            0x7e0cfc18, 0xfe03fc00,                            0x01fffc00, 0xfe0003f8,                            /* upper */                            0x2E4B2E4B, 0x57155715,                            0x99A699A6, 0xE338E338,                            0xFCC0FCC0, 0x00FF00FF,                            0xFF0000FF, 0xFF0000FF,                            /* lower */                            0xD1B4D1B4, 0x57155715,                            0x99A699A6, 0xE338E338,                            0xFCC0FCC0, 0x00FF00FF,                            0xFF0000FF, 0x00FFFF00,             parity_mask = 0x0c             mirroring = F021 } If you value your sanity, do not ask where the constants come from.
    • Some devices, such as TMS570LC4357 Hercules, have a FLASH bank in high memory, and ECC uses the high bits of the address in the ECC calculation. Therefore, we need to extend the participating address bits mask in the linker-generated ECC handling.

      TMS570LC4357 ECC algorithm not supported

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-215 - TMS570LC4357 ECC algorithm not supp...
                SYNCHRONIZED
                • Last Sync Date: