If a host image file is the first object file on the command line, the linker will issue an ABI incompatibility error

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-1051
    • SDSCM00051464
    • PRU_2.1.0
    • PRU_2.1.1
    • Hide
      Reorder the inputs to armcl so that a host image file is not the first
      input.
      Show
      Reorder the inputs to armcl so that a host image file is not the first input.

      If a host image file is the first object file on the command line, the linker will issue an ABI incompatibility error

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            0 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-199 - If a host image file is the first o...
                SYNCHRONIZED
                • Last Sync Date: