c29ofd --call_graph generates a call graph which is missing functions and calls

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium

      The following commands show a contrived single file program, build it, then create the call graph XML file.

      % type file.c
      volatile double v1, v2;
      
      int main()
      {
          return v1 * v2 != 1.0;
      }
      
      % c29clang file.c -o file.out -Wl,-c,-m=file.map
      
      % c29ofd --call_graph file.out > graph.xml
      

      Inspect the call graph in graph.xml. There is no entry for the function main. main is called from the function c_int00_noargs. The function c_int00_noargs appears, and is shown to call yet other functions. But not main. It is likely there are yet other problems similar in nature.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-7020 - c29ofd --call_graph generates a cal...
                SYNCHRONIZED
                • Last Sync Date: