Unable to explicitly build executable project if it is shared between multiple system projects

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium

      It is not possible to explicitly select and build an individual executable project if that project is shared between multiple system projects. However the project will be built if building any of the system projects that reference it.

      This is intended behavior/limitation and an error message should be reported. While Eclipse based CCS reports the error, Theia based CCS suppresses it, whic is a bug.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6944 - Unable to explicitly build executab...
                SYNCHRONIZED
                • Last Sync Date: