Unable to import old CCSv4 projects

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • Code Composer Studio Theia
    • CCSNXT-3538
    • CCS_21.0.0
    • None
    • Import the project using a later CCS Eclipse version (like 12.8) and then importing that project to CCS Theia.

      Unable to import old CCSv4 projects. The project format changed in CCSv5 where .cproject replaced .cdtbuild and .cdtproject and these projects can be imported fine.

      One workaround is to import the project using a later CCS Eclipse version (like 12.8) and then importing that project to CCS Theia.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6878 - Unable to import old CCSv4 projects
                SYNCHRONIZED
                • Last Sync Date: