"Reconnecting to TI Cloud Agent" error occurs when trying to connect to a core on the AM62D AUDIO EVM

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Not Prioritized

      "Reconnecting to TI Cloud Agent" error occurs when trying to connect to a core on the AM62D AUDIO EVM. The issue seems to be specific to AM62D_AUDIO_EVM selection in the Board/Device list for the target configuration. When selecting an AM62A variant, there is no issue with connection (even when using the same board).

      This issue appears to only occur on Linux host environments.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6840 - "Reconnecting to TI Cloud Agent" er...
                SYNCHRONIZED
                • Last Sync Date: