tinyml-1.4.0: Cannot build f28p55 motor bearing fault classification live preview project

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Edge AI Studio
    • EDGEST-1870
    • EAIS_1.7.0
    • EAIS_1.8.0
    • None

      1. Import a 'Motor Bearing Fault Classification' in Edge AI Studio
      2. Run training session using 1.4.0 tinyml with all default parameters using the F28P55
      3. Go to 'Live Preview', and select the completed training run
      4. Click 'Load Program' 
      5. Build fails with attached error

      Note that if you try the same steps using a model created from tinyml 1.3.0, there are no issues with Live Preview. There is also no issue building the project out of the box. Therefore, this appears to be an issue with the model created with tinyml 1.4.0.  

       

      REASON:

      The build errors are caused by changes in the new TVM compiler, which are not yet supported in the current ASM SDKs. Support is planned for the C2000 DPSDK and C2000 MCSDK by November 2026.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6837 - tinyml-1.4.0: Cannot build f28p55 m...
                SYNCHRONIZED
                • Last Sync Date: