When setting a breakpoint via a MCP call the agent should be informed where it was set

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Code Composer Studio Theia
    • CCSNXT-3499
    • CCS_20.5.0
    • CCS_21.1.0
    • None

      It is common for a source line not to be valid for a breakpoint. Maybe it was optimized out. What happens is that the debugger shifts the breakpoint to the next valid line. The agent should know where the breakpoint was actually set so that it is not confused when the halt occurs at a different location than it intended.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6797 - When setting a breakpoint via a MCP...
                SYNCHRONIZED
                • Last Sync Date: