Callbacks registered in the python scripting console aren't evaluated while the console is idle

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Composer Studio Debugger
    • CCBT-3785
    • CCS_21.0.0
    • CCS_21.0.1
    • Generic

      If a callback (or any listener for a debugger event) is registered in the scripting console, it is only serviced while the console is blocked waiting on some scripting call.

      The only exception is if a script is loaded using the console API for loading a file (not the loadFile function in the console). In that case, the script is loaded on a separate thread and that thread handles the events.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6793 - Callbacks registered in the python ...
                SYNCHRONIZED
                • Last Sync Date: