Launch config properties not auto-populated when no launch config exists

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Code Composer Studio Theia
    • CCSNXT-3477
    • CCS_21.0.0
    • CCS_21.0.1
    • None

      • Import an example project with the following in its .projectspec:
        <property name="launch.loadSymbolsOnly" value="true"/>
      • Debug the project with no launch configurations in the current workspace.

      It would be expected that the automatically generated launch configuration to include the loadSymbolsOnly property - this is not the case. This does work when there are already launch configurations in your workspace.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6791 - Launch config properties not auto-p...
                SYNCHRONIZED
                • Last Sync Date: