SysConfig MCP session can get out of sync with file on disk

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Code Composer Studio Theia
    • CCSNXT-3396
    • CCS_20.5.0
    • CCS_21.0.1
    • None

      When deleting an existing project from the workspace and then importing the same project again, Claude (interacting with the MCP server) can think that the configuration from the previous project is present. It could be that it is because the files are open in the editor. That gets out of sync with the actual file.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6685 - SysConfig MCP session can get out o...
                SYNCHRONIZED
                • Last Sync Date: