New UI - device information in train wizard is not correct

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • Edge AI Studio
    • EDGEST-1780
    • EAIS_1.6.1
    • EAIS_2.0.0
    • None

      in train wizard, device information is not correct 

      1. for a project created for a certain extension version (e.g. 1.2.0), the device information shown is not relevant to that version
      2. for a project that is not created for a certain extension version, the device information shown is not relevant to the latest version.

      Test with P55. Note the device information is pulled from 1.0.1. 
      In #1 above, content should be from 1.2.0 (This can be discussed whether it should be 1.3.0) but it should not be from 1.0.1
      In #2, content should be from latest version. (1.3.0 ATM)

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-6684 - New UI - device information in trai...
                SYNCHRONIZED
                • Last Sync Date: