PowerVR Vulkan driver crash using MPV

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Linux Core SDK
    • LCPD-47070
    • 12.00.00
    • 12.01.00
    • am62pxx_sk-fs

      The crash is in libpvr_mesa_wsi.so (PowerVR's Mesa Window System Interface library, part of ti-img-rogue-umlibs v25.3.6908880). The call chain every time is:

        mpv → libplacebo (pl_swapchain_resize) → libvulkan → libpvr_mesa_wsi.so → libVK_IMG.so → SIGSEGV

      pl_swapchain_resize is libplacebo's call to create or resize the Vulkan swapchain - the chain of GPU framebuffers used for presentation to the display. The PowerVR WSI implementation has a NULL pointer dereference somewhere in its vkCreateSwapchainKHR path. This happens in two scenarios:

        1. Without WAYLAND_DISPLAY: crashes immediately during Vulkan instance/surface probing before any playback starts
        2. With WAYLAND_DISPLAY: crashes on the first actual frame render when libplacebo calls pl_swapchain_resize to set up the swapchain for the video dimensions

      This is a bug in the TI/IMG userspace driver - the WSI should return VK_ERROR_INITIALIZATION_FAILED or VK_ERROR_SURFACE_LOST_KHR instead of dereferencing a null pointer.

      To recreate you can run the following command:

      XDG_RUNTIME_DIR=/run/user/1000 WAYLAND_DISPLAY=wayland-1 mpv --vo=gpu --gpu-api=vulkan --hwdec=auto --vd=hevc_v4l2m2m --no-correct-pts --container-fps-override=60 /home/vids/bbb_1080p60_30s.h265

      I ran this as well in gdb to get the following backtrace

      Command: XDG_RUNTIME_DIR=/run/user/1000 WAYLAND_DISPLAY=wayland-1 gdb --args mpv --vo=gpu --gpu-api=vulkan --hwdec=auto --vd=hevc_v4l2m2m --no-correct-pts --container-fps-override=60 /home/vids/bbb_1080p60_30s.h265

      (gdb) run

      (gdb) bt

      Thread 15 "vo" received signal SIGSEGV, Segmentation fault.
      [Switching to Thread 0xffffc7ffef60 (LWP 8259)]
      0x0000ffffe8ed1d98 in ?? () from /usr/lib/libVK_IMG.so
      (gdb) bt
      #0  0x0000ffffe8ed1d98 in ?? () from /usr/lib/libVK_IMG.so
      #1  0x0000ffffc4175aec in ?? () from /usr/lib/libpvr_mesa_wsi.so
      #2  0x0000ffffc417670c in ?? () from /usr/lib/libpvr_mesa_wsi.so
      #3  0x0000ffffc417401c in ?? () from /usr/lib/libpvr_mesa_wsi.so
      #4  0x0000ffffc417a234 in ?? () from /usr/lib/libpvr_mesa_wsi.so
      #5  0x0000ffffc4174808 in ?? () from /usr/lib/libpvr_mesa_wsi.so
      #6  0x0000fffff49a7fc8 in ?? () from /usr/lib/libvulkan.so.1
      #7  0x0000fffff522c090 in ?? () from /usr/lib/libplacebo.so.351
      #8  0x0000fffff522ca8c in ?? () from /usr/lib/libplacebo.so.351
      #9  0x0000fffff520360c in pl_swapchain_resize () from /usr/lib/libplacebo.so.351
      #10 0x0000aaaaaabf8fd4 in ?? ()
      #11 0x0000aaaaaabf96fc in ?? ()
      #12 0x0000aaaaaabc19e8 in ?? ()
      #13 0x0000aaaaaabc028c in ?? ()
      #14 0x0000fffff4832b58 in start_thread (arg=0xffffc7ffef60) at pthread_create.c:454
      #15 0x0000fffff48969dc in thread_start () at ../sysdeps/unix/sysv/linux/aarch64/clone3.S:75

      This command works so i know it's a vulkan issue: 

      XDG_RUNTIME_DIR=/run/user/1000 WAYLAND_DISPLAY=wayland-1 mpv --vo=gpu --gpu-api=opengl --hwdec=auto --vd=hevc_v4l2m2m --no-correct-pts --container-fps-override=60 /home/vids/bbb_1080p60_30s.h265
       

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6562 - PowerVR Vulkan driver crash using MPV
                SYNCHRONIZED
                • Last Sync Date: