Compiler error parser does not recognize TIClang error for missing .opt file

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Composer Studio Theia
    • CCSNXT-3321
    • CCS_20.5.0
    • CCS_20.5.1
    • None

      TIClang compiler generates an error for a missing .opt file, but this error's text does not match any of the compiler error parser's regex'es, so it does not generate an error marker.

      1. Create any ARM TIClang project
      2. Open project Properties, then on page Build > Tools > Compiler > Advanced Options > Command Files, add a non-existent .opt file to the list
      3. Build the project
      4. -> The missing .opt file generates an error in the build-output
      5. -> The error is coloured in red in Output view
      6. -> But it does not show up in the Problems view

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6544 - Compiler error parser does not reco...
                SYNCHRONIZED
                • Last Sync Date: