Breakpoints should be resolved after adding source resolution hints

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Implemented
    • Priority: Medium
    • Code Composer Studio Debugger
    • CCBT-3743
    • CCS_21.0.0
    • Generic

      With current implementation, if a source breakpoint is set and then source resolution hints for that file is added, the breakpoints don't get enabled. This is because it is expected that source resolution hints to be added first before setting breakpoints.

      The breakpoints should get resolved and enabled after we add source hints.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-6461 - Breakpoints should be resolved afte...
                SYNCHRONIZED
                • Last Sync Date: